To set the taps using a SCPI command, refer to the command under the Multipath description.
Click this button and remove the selected multipath tap.
Indicating the tap index.
Click the check box to enable or disable a specific tap.
Range: 0 – 100 chips
Default: 1
Enter the delay offset of the tap to the line-of-sight signal.
The unit chip refers to the chip width of the system:
Range: -40 dB to 0 dB
Default: -10 dB
Enter the power offset of the tap to the line-of-sight signal.
Range: -125 kHz to 125 kHz
Default: 5 Hz
Enter the Doppler shift of the tap to the line-of-sight signal.